AXIS#.MT.V

Description

AXIS#.MT.V specifies the motion task velocity. This is the maximum speed the axis will use when moving to the target position. The axis will accelerate up to this speed and stay at this speed before decelerating to a stop at the desired position. The axis may not get to this speed if the distance is short.

The motion task velocity is also limited by AXIS#.VL.LIMITP or AXIS#.VL.LIMITN depending on the direction of the motion task.

By default AXIS#.MT.V is zero and will generate an error if you try to start the motion task with AXIS#.MT.MOVE. You have to set AXIS#.MT.V to a non-zero value before this motion task can be started.

Examples

Code

Sets the velocity of motion task 0 to 60 RPM. The first parameter is the motion task number and the second is the velocity.

-->AXIS1.MT.V 0 60

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read Only Array

Units

Rotary: RPM, RPS, deg/s, (custom units)/s, rad/s

See Velocity Units for details.

Range

Depends on units. See Velocity Range for details.

Default Value

0 RPM

Depends on units. See Velocity Units for details.

Data Type

Float

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.MT.V 0

50d3h

01h

Signed32

Velocity

-

Read/Write

No

AXIS1.MT.V 1

50d3h

02h

Signed32

Velocity

-

Read/Write

No

AXIS1.MT.V 2

50d3h

03h

Signed32

Velocity

-

Read/Write

No

AXIS1.MT.V 3

50d3h

04h

Signed32

Velocity

-

Read/Write

No

AXIS1.MT.V 4

50d3h

05h

Signed32

Velocity

-

Read/Write

No

AXIS1.MT.V 5

50d3h

06h

Signed32

Velocity

-

Read/Write

No

AXIS1.MT.V 6

50d3h

07h

Signed32

Velocity

-

Read/Write

No

AXIS1.MT.V 7

50d3h

08h

Signed32

Velocity

-

Read/Write

No

AXIS1.MT.V 8

50d3h

09h

Signed32

Velocity

-

Read/Write

No

AXIS1.MT.V 9

50d3h

0ah

Signed32

Velocity

-

Read/Write

No

AXIS1.MT.V 10

50d3h

0bh

Signed32

Velocity

-

Read/Write

No

AXIS1.MT.V 11

50d3h

0ch

Signed32

Velocity

-

Read/Write

No

AXIS1.MT.V 12

50d3h

0dh

Signed32

Velocity

-

Read/Write

No

AXIS1.MT.V 13

50d3h

0eh

Signed32

Velocity

-

Read/Write

No

AXIS1.MT.V 14

50d3h

0fh

Signed32

Velocity

-

Read/Write

No

AXIS1.MT.V 15

50d3h

10h

Signed32

Velocity

-

Read/Write

No

AXIS1.MT.V 16

50d3h

11h

Signed32

Velocity

-

Read/Write

No

AXIS1.MT.V 17

50d3h

12h

Signed32

Velocity

-

Read/Write

No

AXIS1.MT.V 18

50d3h

13h

Signed32

Velocity

-

Read/Write

No

AXIS1.MT.V 19

50d3h

14h

Signed32

Velocity

-

Read/Write

No

AXIS1.MT.V 20

50d3h

15h

Signed32

Velocity

-

Read/Write

No

AXIS1.MT.V 21

50d3h

16h

Signed32

Velocity

-

Read/Write

No

AXIS1.MT.V 22

50d3h

17h

Signed32

Velocity

-

Read/Write

No

AXIS1.MT.V 23

50d3h

18h

Signed32

Velocity

-

Read/Write

No

AXIS1.MT.V 24

50d3h

19h

Signed32

Velocity

-

Read/Write

No

AXIS1.MT.V 25

50d3h

1ah

Signed32

Velocity

-

Read/Write

No

AXIS1.MT.V 26

50d3h

1bh

Signed32

Velocity

-

Read/Write

No

AXIS1.MT.V 27

50d3h

1ch

Signed32

Velocity

-

Read/Write

No

AXIS1.MT.V 28

50d3h

1dh

Signed32

Velocity

-

Read/Write

No

AXIS1.MT.V 29

50d3h

1eh

Signed32

Velocity

-

Read/Write

No

AXIS1.MT.V 30

50d3h

1fh

Signed32

Velocity

-

Read/Write

No

AXIS1.MT.V 31

50d3h

20h

Signed32

Velocity

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6309

1

6309 (0x18a5)

AXIS1.MT.V

Signed32[32]

Read/Write

Yes

71845

2

6309 (0x18a5)

AXIS2.MT.V

Signed32[32]

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.MT.V

6309

Float[32]

Read/Write

Velocity

Related Topics

Motion Tasks